RFTapData

The following table describes the attribute editing configuration options for each field, separated into these categories:

  • Can the Editable setting be changed?

    • This column answers the question, “Am I allowed to add or remove this field from Attribute Editor?” The default for the Editable tag is Editable=“false.” If the table below states “Yes,” then you are allowed to add the tag Editable=“true” to that field, if desired. It then appears in Attribute Editor in the application. Editable fields are inherently Viewable, even if the Viewable setting is not included in the schema.xml.

  • Can the Viewable setting be changed?

    • This column answers the question, “Am I allowed to add or remove this field from being viewed in Attribute Editor?” To do so, add the tag Viewable=“true.” Viewable fields do not have to be Editable. In other words, you can provide them to your users in a read-only mode. A “No” in the table below means the value from that field is presented to the user in another, more meaningful way than the raw data contained in the field, and you cannot change its viewable setting.

  • Are attributes imported from GIS?

    • A “Yes” in the table below means the data originate from the GIS. These fields should have a tag of Import=“true”, and that tag should not be changed in the schema.xml.

    • A “No” in the table below means the field is populated while working in the application.

  • Data Type

    • Because the default data type is “string,” notice that most of the entries in the table below state “Not Required.” This is because if you do not add a DataType tag, it uses the default string type.

  • Validation Options

    • Validation Options only apply to Editable fields. Because most of the fields are managed by the application, notice that most options in the table below state “None.”

  • Coded Domain Name

    • This lists the domain provided in the default schema.xml.

  • Notes

    • This column includes other information for that field.

Field Name (CoaxName)

Can Editable setting be changed?

Can Viewable setting be changed?

Are attributes imported from GIS?

Data Type

Validation Options

Coded Domain Name

Notes

EsriId

No

Yes

Yes

Not Required

None

   

NetworkId

No

Yes

Yes

Not Required

None

   

AerialStructureId

No

Yes

Yes

Not Required

None

   

CatalogId

No

Yes

Yes

Not Required

None

   

CreationUser

No

Yes

Yes

Not Required

None

 

Importing this value is optional. Regardless of whether it is imported or not, DHFC sets the value when data are pushed to GIS.

ConditioningPluginCID

No

Yes

Yes

Not Required

None

 

This field is required only if your company is using plugins. If you are not using plugins, this field is optional.

Regarding the Viewable setting, information about the plugin is always visible in the Conditioning Plugins section on the Device pane. No configuration is needed to see information on the Device pane. Set this value to “true” if you also want to see the information in Attribute Editor.

ConditioningPlugin-ModelNumber

No

Yes

Yes

Not Required

None

 

This field is required only if your company is using plugins. If you are not using plugins, this field is optional.

Regarding the Viewable setting, information about the plugin is always visible in the Conditioning Plugins section on the Device pane. No configuration is needed to see information on the Device pane. Set this value to “true” if you also want to see the information in Attribute Editor.

ConditioningPluginType

No

Yes

Yes

CodedValueDomain

None

RFConditioning-PluginTypes

This field is required only if your company is using plugins. If you are not using plugins, this field is optional.

Regarding the Viewable setting, information about the plugin is always visible in the Conditioning Plugins section on the Device pane. No configuration is needed to see information on the Device pane. Set this value to “true” if you also want to see the information in Attribute Editor.

ConditioningPluginValue

No

Yes

Yes

Not Required

None

 

This field is required only if your company is using plugins. If you are not using plugins, this field is optional.

Regarding the Viewable setting, information about the plugin is always visible in the Conditioning Plugins section on the Device pane. No configuration is needed to see information on the Device pane. Set this value to “true” if you also want to see the information in Attribute Editor.

DateCreated

No

Yes

Yes

Not Required

None

 

Importing this value is optional. Regardless of whether it is imported or not, DHFC sets the value when data are pushed to GIS.

DateModified

No

Yes

Yes

Not Required

None

 

Importing this value is optional. Regardless of whether it is imported or not, DHFC sets the value when data are pushed to GIS.

FedFromComponentId

No

Yes

Yes

Not Required

None

   

Flipped

No

Yes

No

Not Required

None

   

ForwardDropSignalHigh

No

No

No

Not Required

None

   

ForwardDropSignalLow

No

No

No

Not Required

None

   

ForwardOutputHighLevel

No

No

No

Not Required

None

   

ForwardOutputLowLevel

No

No

No

Not Required

None

   

FrequencyRange

No

No

No

Not Required

None

   

InternalPowerMapping

No

No

Yes

Not Required

None

   

InventoryNum

No

Yes

No

Not Required

None

   

IsEndOfLine

No

Yes

No

Not Required

None

   

IsInMdu

No

Yes

Yes

Not Required

None

   

IsLocked

No

Yes

Yes

Not Required

None

 

The lock button on the device pane toggles the state of this property.

IsPTap

No

Yes

No

Not Required

None

   

IsSelfTerminating

No

Yes

No

Not Required

None

   

LastUser

No

Yes

Yes

Not Required

None

 

Importing this value is optional. Regardless of whether it is imported or not, DHFC sets the value when data are pushed to GIS.

Manufacturer

No

Yes

No

Not Required

None

   

ModelNumber

No

Yes

No

Not Required

None

   

Name

Yes

Yes

Yes

Not Required

MaxLength

 

This field does not appear in Attribute Editor, but is editable at the top of the device pane.

The default value can be null.

PortCount

No

Yes

No

Not Required

None

   

PoweringFedFromComponentId

No

Yes

Yes

Not Required

None

   

ReturnSignalHighFrequency

No

No

No

Not Required

None

   

ReturnSignalHighLevel

No

No

No

Not Required

None

   

ReturnSignalLowFrequency

No

No

No

Not Required

None

   

ReturnSignalLowLevel

No

No

No

Not Required

None

   

SpecSymbology

No

Yes

No

Not Required

None

   

SymbolRotation

Yes

Yes

Yes

double

Range

   

TapValue

No

Yes

No

Not Required

None

   

UGStructureId

No

Yes

Yes

Not Required

None

   

Workflow_Status

Yes

Yes

Yes

Not Required

None

WorkflowState

 
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?