RFPad_RFAmplifier_Fwd
There are two versions of this relationship:
-
RFPad_RFAmplifier_Fwd for the as-built representation.
-
RFPad_RFAmplifier_Fwd_D for the in-design representation.
RFPad_RFAmplifier_Fwd, the As-Built Relationship
|
Relationship Class Property |
Value or Choice |
|---|---|
|
Name |
RFPad_RFAmplifier_Fwd |
|
Origin Table or Feature Class |
RFPad |
|
Destination Table or Feature Class |
RFAmplifier |
|
Relationship Type |
Simple |
|
Forward Label |
RFAmplifier |
|
Backward Label |
RFPad |
|
Message Direction |
None (no messages propagated) |
|
Cardinality |
1–M (one to many) |
|
Relationship Attributes |
No, I do not want to add attributes to this relationship class. |
|
Primary Key |
NetworkId |
|
Foreign Key |
ForwardPadId |
RFPad_RFAmplifier_Fwd_D, the Design Relationship
|
Relationship Class Property |
Value or Choice |
|---|---|
|
Name |
RFPad_RFAmplifier_Fwd_D |
|
Origin Table or Feature Class |
RFPad_D |
|
Destination Table or Feature Class |
RFAmplifier_D |
|
Relationship Type |
Simple |
|
Forward Label |
SECom.ARCFM.RFAmplifier |
|
Backward Label |
SECom.ARCFM.RFPad |
|
Message Direction |
None (no messages propagated) |
|
Cardinality |
1–M (one to many) |
|
Relationship Attributes |
No, I do not want to add attributes to this relationship class. |
|
Primary Key |
NetworkId |
|
Foreign Key |
ForwardPadId |