GEX2563900-02

Avoid Condensation

To ensure the specified insulating level, the switchgear panel – especially its insulating components – must not be exposed to condensation.

Measures to take in case of condensation

  • Should condensation be detected in or on the panel, clean the panel in accordance with Cleaning .

  • Installation or inspection of panel heating. It must provide a sufficient heating performance to prevent condensation on the panel.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.