GEX2563900-02

Operating the Circuit Breaker Manually

Switching ON via the Operating Rod

Insert the operating rod into the right-hand guide of the front door and press it right to the back (Figure 21, 1). The circuit breaker is switched ON; the position indicator indicates ON (2).

The energy storing device can be charged again immediately after switching ON (by motor). If supply voltage is present, the energy storage device is charged automatically.

Figure 21
Switching the Circuit Breaker ON via the Operating Rod

1

Operating rod

2

Position indicator reads: Circuit breaker ON

Switching OFF via the Operating Rod

Insert the operating rod into the left-hand guide of the front door and press it right to the back (Figure 22, 1). The circuit breaker is switched OFF. The position indicator indicates OFF (2).

Figure 22
Switching the Circuit Breaker OFF via the Operating Rod

1

Operating rod

2

Position indicator reads: Circuit breaker OFF

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.