GEX2563900-02

Disposal After the End of the Useful Life

A material and recycling data sheet can be provided on request for the disposal of series EasySet MV switchgear at the end of its service life.

Disposal is performed as a service by the manufacturers service center which to payment.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.