GEX2563900-02

Racking-Out the Truck from Service into Disconnected Position

Follow the below steps to racking-out the truck from service into disconnected position:

  1. Open cover (Figure 25, 1) and insert crank (2).

  2. Turn crank counter-clockwise (3) until the truck has been racked out. Remove crank.

  3. Check position of truck (Figure 26) through the inspection glass.

 

Figure 25
Racking-Out the Truck

 

Figure 26
Truck in Disconnected Position

1

Open cover

2

Insert crank

3

Turn crank counter-clockwise

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.