GEX2563900-02

Padlocks (not Included in Scope of Supplies)

The bore holes are provided for padlock yokes of Ø 8 mm.

Figure 18
Circuit Breaker Padlock

Cover flaps on ON/OFF push button for the circuit breaker can be locked by means of a padlock (optional).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.