GEX2563900-02

Racking-In the Truck from Disconnected into Service Position

Follow the below steps to racking-in the truck from disconnected into service position:

  1. Open cover (Figure 23, 1) and insert crank (2).

  2. Turn crank clockwise (3) until the truck has been racked in. Remove crank.

  3. Check position of truck (Figure 24) through the inspection glass.

 

Figure 23
Racking-In the Truck

 

Figure 24
Truck in Service Position

1

Open cover

2

Insert crank

3

Turn crank clockwise

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.