GEX2563900-02

Servicing Schedule

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
In case of frequent condensation or air pollution (dust, smoke, or corrosive gases), the maintenance intervals must be adapted to the actual conditions.
Failure to follow these instructions will result in death or serious injury.

We recommend performing a visual inspection of the panels at least every four years, depending on the strain to which they are subjected during operation and the operating conditions.

For cleaning and maintenance work, refer to Access to the Main Circuit Compartments, Access to the cable compartment, switching device compartment and the busbar compartment in Installation Manual (GEX2564100).

In case of ambiguities or irregularities, contact the manufacturers service center immediately.

Circuit Breaker Switch Cubicle / Mainly recommended for maintenance activities

Preventive maintenance activities

Minimal frequency(1) / Performance level

  Y1 Y2 Y3 Y4 Y5 Y6 Y7 Y8 Y9 Y10

LV Compartment

Inspection of auxiliaries equipment

Inspection of wiring connections (tightening, fixing)

Cubicle

Cleaning cubicle / internal equipment

Inspection of the position indicators and signalling micro switches

Inspection of locking + interlocking mechanism function

 

 

 

 

 

Inspection of withdrawal mechanism

 

 

 

 

 

Inspection of the shutters

 

 

 

 

 

Cleaning / checking switch line operating mechanism

     

     

   

Cleaning / checking of isolators (tightening, chalking, cracking, signs of heating)

     

     

   

Cleaning / checking of earthing switch operating mechanism

     

     

   

Cleaning / checking / greasing of earthing switch plugs

     

     

   

Cleaning / checking / greasing of shutter locking system

     

     

   

Cables compartment

Inspection of cables (chalking, signs of heating)

Inspection of wiring connections (tightening, fixing)

CT / VT compartment

Cleaning / inspection of isolators (chalking, cracking, signs of heating)

     

     

   

Cleaning / inspection of TPs (tightening, chalking, cracking, signs of heating)

     

     

   

Busbar compartment

Inspection of busbars (cleaning, tightening, chalking, cracking, signs of heating)

     

     

   

Inspection of isolator switches (cleaning, tightening, chalking, cracking, signs of heating)

     

     

   

Circuit breaker

General state: visual checking, cleanliness, insulator condition, oxidation, no corrosion of supporting structure

Checking of number of operation

Cleaning of resin bodies

Inspection of state of the auxiliaries contact (on/off, rack in, rack off etc.)

Inspection of functional and safety interlock on device

Cleaning / checking / greasing of the power contacts (plugs, sliding contact, light greasing)

     

     

   

Measurement of main contact resistance (microhmeter)

     

     

   

Cleaning / checking / greasing of the moving withdrawable parts

     

     

   

Checking of coupling rods

     

     

   

Cleaning / checking / greasing of the operating mechanism

     

     

   

Cleaning / checking / greasing of the latching mechanism

     

     

   

Cleaning / checking / greasing of the closing and opening springs

     

     

   

Cleaning / checking / greasing of the motor and reduce

     

     

   

Cleaning / checking / greasing of all linkages

     

     

   

Check LV electrical wiring connections

     

     

   

Tests

Mechanical (manual on/off)

Electrical (remote on/off)

Associated protection

Inspection of protection relay (setting, tripping functions)

     

     

   

Inspection of upstream / downstream selectivity

     

     

   

Schneider Electric Proprietary Diagnosis services offers

Diagnosis to detect drifts from the initial state and significant trends, to anticipate on the corrective action (future failures) required to ensure equipment safety and continuity of service, and plan the action for the most convenient time for customer operations.

ProDiag Breaker Monitors opening / closing / spring-loading operations drifts

     

     

   

Checking / adjusting of condition of the damper and / or stop device

     

     

   

Checking of opening / closing times and speeds

     

     

   

Checking of charging time

     

     

   

Checking of contact synchronization

     

     

   

Checking of safety to close (overtravel and stabilisation)

     

     

   

Checking of safety to open (overtravel and stabilisation)

     

     

   

ProDiag Corona Surface or internal partial discharges detection.

     

     

   

Spare Parts

Secure: Parts commonly used in corrective maintenance interventions

Relay, LV Fuse

Light maintenance

Auxiliary contact

Light maintenance

Tripping coil

Light maintenance

Mitop for switch

Light maintenance

Undervoltage coil

 

Advanced maintenance

Motor

 

Advanced maintenance

Prevent: Parts whose condition are checked in preventive maintenance interventions

Gear motor

     

Exclusive maintenance

Operating mechanism

     

Exclusive maintenance

Life extension: Parts to extend the life of the equipment

Capacitive insulator

 

Advanced maintenance

Earthing clusters

 

Advanced maintenance

(1) Recommended under optimal operating conditions. However this recommended frequency should be increased according to
a) the level of criticality (low, major, critical) and
b) the severity of environment conditions (for example, corrosive, naval, offshore) following the prescriptions of manufacturer’s services.

Exclusive maintenance conducted by ED equipment manufacturer only.

Advanced maintenance, preferably conducted by ED equipment manufacturer or manufacturer certified partner.

● Light maintenance, conducted by ED equipment manufacturer or customer competent technician.

Schneider Electric ranges covered by this Maintenance guide: MCset, EasySet MV, SM6, Fluokit, VM6, Fluair, DNF, Alliance.

Does not supersede the information provided in the product user guide.

Metering Cubicle / Mainly recommended for maintenance activities

Preventive maintenance activities

Minimal frequency(1) / Performance level

  Y1 Y2 Y3 Y4 Y5 Y6 Y7 Y8 Y9 Y10

LV Compartment

Inspection of connections

Checking of wiring

Equipment compartment

Cleaning / checking of active part and enclosure (chalking, cracking, signs of heating)

Cleaning / checking of isolators (chalking, signs of heating)

Checking of lock and inter-lock system

Checking of auxiliaries contacts position indicator

Cleaning / checking of operating mechanism

     

     

   

Cleaning / checking of the earthing switch operating mechanism

     

     

   

Fuses

Inspection of fuse (chalking, color, cracking, corrosion)

Inspection of fuse fixing

Inspection of fuse signaling microswitch

Inspection of fuse striker

Busbar compartment (power off)

Inspection of busbars (signs of heating)

     

     

   

Inspection of isolator switches (chalking, signs of heating)

     

     

   

CT / VT compartment

Cleaning / inspection of isolators (tightening, chalking, cracking, signs of heating)

     

     

   

Cleaning or/ inspection of TPs (tightening, chalking, cracking, signs of heating)

     

     

   

Tests

Mechanical (manual on/off)

Electrical (remote on/off)

Schneider Electric Proprietary Diagnosis services offers

Diagnosis to detect drifts from the initial state and significant trends, to anticipate on the corrective action (future failures) required to ensure equipment safety and continuity of service, and plan the action for the most convenient time for customer operations.

ProDiag Corona Surface or internal partial discharges detection.

     

     

   

ProDiag Fuse Measurement of fuses internal impedance / comparison with manufacturer's data

     

     

   

Spare Parts

Secure: Parts commonly used in corrective maintenance interventions

Auxiliary contact

Light maintenance

Prevent: Parts whose condition are checked in preventive maintenance interventions

Operating mechanism

     

Exclusive maintenance

Life extension: Parts to extend the life of the equipment

Capacitive insulator

 

Advanced maintenance

Earthing and fuses cluster

 

Advanced maintenance

MV Fuse (ProFusion maintenance)

 

Advanced maintenance

(1) Recommended under optimal operating conditions. However this recommended frequency should be increased according to
a) the level of criticality (low, major, critical) and
b) the severity of environment conditions (for example, corrosive, naval, offshore) following the prescriptions of manufacturers services.

Exclusive maintenance conducted by ED equipment manufacturer only.

Advanced maintenance, preferably conducted by ED equipment manufacturer or manufacturer certified partner.

● Light maintenance, conducted by ED equipment manufacturer or customer competent technician.

Schneider Electric ranges covered by this Maintenance guide: MCset, EasySet MV, SM6, Fluokit, VM6, Fluair, DNF, Alliance.

Does not supersede the information provided in the product user guide.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.