GEX2563900-02

Nameplate

The type designation on the nameplates on the front of the panels (see Figure 14) informs about essential technical data. The information below is required when submitting enquiries to the manufacturer or ordering spare parts:

  • Type designation

  • Serial number

  • Year of construction

Figure 14
Nameplate on Panel Front

1

Technical data

3

Serial number

2

Type designation

4

Year of construction

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.