GEX2563900-02

Panel Variants

The sub-chapters always show panel types with the appropriate basic equipment. Customized models with additional equipment are described in the switchgear-specific documentation.

Functional Overview

EasySet MV has a comprehensive range of functions to suit all requirements for many applications.

The table below can be used to link requirements to functional units and gives basic information on the general composition of each unit.

Panel Architecture

Feeder

Bus coupler

Bus riser

Application

Line transformer/generator

Line transformer/motor/capacitor

Bus section coupler

Bus section riser

Main device

Circuit breaker

Circuit breaker

Circuit breaker

Fix copper bar

Type of device

EasyPact EXE

EasyPact EXE

EasyPact EXE

Copper bar

Panel function

Incomer

Outgoing

Bus sectioning

Panel name, code

F

F

BSC

BSR

Single line diagram

Panel Architecture

Metering

Incoming and Outgoing

Application

Line PT

Bus PT

Line and bus PT

ICOG

Main device

Voltage Transformer

Voltage Transformer

Voltage Transformer

Circuit breaker

Type of device

NA

NA

NA

EasyPact EXE

Panel function

Line side voltage metering

Busbar voltage metering

Line side and busbar voltage metering

Single incoming and outgoing panel

Panel name, code

LPT

BPT

BLPT

ICOG

Single line diagram

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.