GEX2563900-02

Dimensions and Weights (Without Packaging)

For the precise panel dimensions, refer to the switchgear-specific documentation. These depend on:

  • Rated voltage

  • Rated normal current

  • Rated short-time current and

  • Additional equipment:

    • Busbar attachments

    • Rear high voltage cable connection

Figure 12
Dimensions of EasySet MV Panels

W

Panel width

H

Panel height (depending on height of low-voltage compartment)

H1

Height of low-voltage compartment

H2

Panel height without low-voltage compartment and attachments

D

Panel depth

Figure 13
Dimensions of Deflector

1

Deflector

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.