GEX2563900-02

Move Truck into Service or Disconnected Position

Trucks may on principle only be moved into service or disconnected position when de-energized.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
  • Switch circuit-breaker OFF or, in case of disconnector truck EasyPact EXE, isolate the feeder.
  • Do not pull the crank out before the truck in question has reached its end position.
  • Do not pull the crank out in an undefined intermediate position.
Failure to follow these instructions will result in death or serious injury.

Initial situation:

  • Circuit breaker OFF

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.