GEX2563900-02

Coupling Busbar Sections via Bus Section Coupler

Coupling the sections (With EasyPact EXE truck)

Initial situation:

  • Circuit breaker: OFF

  • EasyPact EXE truck: In disconnected position


Follow the steps for coupling the sections

  1. Move truck into service position (Figure 28, 1).

  2. Switch circuit breaker ON (2).


Figure 28
Coupling busbar sections via bus section coupler and EasyPact EXE trucks


Uncoupling

Follow the steps for uncoupling the sections

  1. Switch circuit breaker OFF.

  2. Move truck into disconnected position.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.