GEX2563900-02

Environmental and Operating Conditions

@Updated D1

EasySet MV is an indoor switchgear and may only be operated under normal conditions in accordance with IEC 62271-1: 2017.

Operation under conditions deviating from these is only admissible subject to consultation with and written approval from the manufacturer.

Ambient conditions in accordance with IEC 62271-1: 2017

Temperature class

-5 °C Indoors(1)

Ambient temperature minimum or maximum

-5 °C/+45 °C(1)

Average value over 24 hours

≤ 35 °C

Mean relative air humidity: 24 hours/1 month

≤ 95%/≤ 90%

Installation altitude above sea-level

≤1000 m

(1) Higher values available on request.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.