GEX2563900-02

Switching the Circuit Breaker Electrically

Switching ON (Closing)

Actuate closing release via bay computer or remote control.

The energy storing device can be charged immediately after switching ON (by motor). If voltage is applied to the motor, charging is performed automatically.

Switching OFF (Opening)

Follow the below steps to switch off the circuit breaker:

  • Actuate the opening release via the bay computer or the remote control

  • By undervoltage release or

  • By secondary release

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.