GEX2563900-02

Cleaning

WARNING
hazard of incorrect cleaning
  • To ensure the specified insulating level, the insulating components must be clean and dry. On principle, cleanliness deserves utmost attention.
  • When deposited dirt or humidity is detected, the panels must be cleaned in an expert fashion.
  • When performing cleaning, make sure that the lubrication in the drive mechanisms is not removed.
  • If the drive mechanisms are no longer sufficiently lubricated, new lubrication must be applied.
  • The drives must not be disassembled for service and maintenance work.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Slight contamination

  • Clean using a dry, lint-free cloth.

  • Depending on the degree of soiling, replace cloth as often as necessary.


Serious contamination

Use cleaning agent, 1 litre can (see Auxiliary Products ). The use of other cleaning agents is not admissible.

  • Wear protective gloves

  • Use cleaning agent according to manufacturers instructions

  • Soak the cloth thoroughly and wipe the insulating components. Keep duration of exposure as short as possible.

  • Expose the cleaned surface to the air for at least two hours.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.