GEX2563900-02

Electromagnetic Interlocks (Optional)

WARNING
HAZARD OF IMPROPER OPERATION
Locking of the switchgear interlocking must be complete to avoid detected error.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTE:
  • If the supplied voltage has a phase fault, all electrical interlocks are in the locked position. Measure: Re-establish supply voltage.

  • Note the purchase contract and the switchgear specific circuit diagram as regards the design of the interlocking systematics.

NOTICE
Hazard of incorrect operating conditions
If no blocking coils are being used for the locking devices, a mechanical lock-out with cylinder or U lock must be provided.
Failure to follow these instructions can result in equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.