Technical Data of Electrical Control and Operating Devices
The switchgear panels have been designed on principle so as to permit manual operation.
The drive mechanisms of the individual switching devices can be equipped, depending on the specific customer‘s model, with additional electrical control and operating devices. These are defined in the switchgear-specific circuit diagram (see switchgear documentation).
Component fitting options:
-
Auxiliary switches are always actuated directly by the truck or by the switch shaft via an intermediate linkage. Their position always corresponds to that of the main contacts. The switching functions have been set in the factory according to the circuit diagram.
-
Micro-switches are used depending on the customized panel models.
|
Description |
Overview of rated supply voltages (V) |
|||||
|---|---|---|---|---|---|---|
|
Direct voltage DC |
24 |
48 |
60 |
110 |
125 |
220 |
|
Alternating voltage AC |
(110)/120 |
(220)/230 |
||||
Trucks
Electrical control and operating devices of trucks are described in the appropriate Technical Manuals (1).
(1) Contact to Schneider Electric Sales team.