GEX2563900-02

Operating Specifications

DANGER
Hazard of ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
  • The switchgear unit may only be operated by specialist electricians who have proven experience (training certificate) in conjunction with the EasySet MV Standard series and all the relevant safety standards. Refer to the Safety Provisions.
  • To rule out incorrect switching operations, the operating sequences described below must be complied with.
  • Complete each switching operation.
  • Check whether the supply voltage is ON.
  • After each switching operation for which you have used a crank or a lever, remove this tool and store it in the tool board.
Failure to follow these instructions will result in death or serious injury.
CAUTION
hazard of incorrect operation
In case supply voltage is not available:
  • Check if blocking coils (locking the interrogation slides and circuit breaker pushbuttons, depending on design) are in locked position.
  • Check if an undervoltage release (optional) has dropped out.
  • Re-establish the supply voltage.
Failure to follow these instructions can result in injury or equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.