GEX2563900-02

Switching a Feeder

Initial situation:

  • Circuit breaker: OFF

  • EasyPact EXE truck: In disconnected position


Switch feeder cable ON

Follow the below steps to switch feeder cable ON:

  1. Move truck into service position (Figure 27,1).

  2. Switch circuit breaker ON (2).

Figure 27
Switch feeder cable ON

Switch feeder cable OFF

Follow the below steps to switch feeder cable OFF:

  1. Switch circuit breaker OFF.

  2. Move truck into disconnected position.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.