990-91407D-001

Configure Life Cycle Monitoring

  1. From the home screen on the display select Service > LCM settings.
  2. Set the Air filter check (months) - time in months between air filter checks. The system will generate a Check air filter message when it is time to check the air filters.
    NOTE: The Air filter check (months) is set to 0 when no air filters are installed.
  3. When an air filter has been replaced, reset the Air filter counter (days).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?