990-91407D-001

Status Indicators of the SPDs

When the front door on the UPS is open, the status indicators (A) of the SPDs are visible. When the status indicator on one of the SPDs turns red, the SPD is inoperable and needs to be replaced. Please contact Schneider Electric for service.

NOTE: It is recommended to check the status of the SPDs every 6 months.

Front view of the SPDs

Placement of the SPDs on the 3:1 UPSs

10-40 kVA 3:1 220 VDC UPS

50-80 kVA 3:1 220 VDC UPS

100-120 kVA 3:1 220 VDC UPS

 

10-40 kVA 3:1 384 VDC UPS

60-80 kVA 3:1 384 VDC UPS

Placement of the SPDs on the 3:3 UPSs

10-80 kVA 3:3 384 VDC UPS

100-120 kVA 384 VDC 3:3 UPS

160-200 kVA 3:3 384 VDC UPS

 
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?