Configure the Electrical Settings
| NOTICE |
|---|
|
risk of equipment damage
Only trained personnel having completed the required training
must make modifications to the UPS system parameters.
Failure to follow these instructions can result in equipment damage.
|
- From the home screen of the display select and configure
the following:
- Operation mode: Choose between Single for single system and Parallel for parallel system.
- ECO mode: Select if ECO mode should be enabled or disabled. For more information on ECO mode, see ECO Mode.
- Bypass not allowed: When this setting is enabled, the UPS will not be allowed to transfer to bypass operation.
- Auto restart: Select if Auto restart should be enabled or disabled. For more information on auto restart, see Auto Restart.
- Frequency converter mode: Select if Frequency converter mode should be enabled or disabled. For more information on frequency converter mode, see Frequency Converter Mode.
- Tap Save settings.
- Tap the arrow down symbol and configure the following:
- INV ON without battery connected: When this setting is enabled, the UPS can be started and can supply the load without any batteries connected. When this setting is disabled, the UPS can only be started if batteries are connected.
- Bypass overload curve protection: When this setting is enabled, the UPS will turn off and disconnect
the load in case of an overload on the bypass to protect the UPS.
When this setting is disabled, the UPS will stay in bypass mode and
supply the load during an overload on the bypass.
NOTICE Risk of equipment damageWhen Bypass overload curve protection is disabled, the UPS may sustain damage during an overload on the bypass.Failure to follow these instructions can result in equipment damage. - INV output short - transfer to bypass: When this setting is enabled, the UPS will transfer to bypass instead of disconnecting the output in case of a short circuit on the inverter output.
- Tap Save settings.