990-91407D-001

View System Status Information

  1. From the home screen of the display select Status.
  2. You can now select to view status for:
    • Input status: Phase voltage, phase-to-phase voltage, frequency, and operating status.
    • Output status: Phase voltage, phase-to-phase voltage, frequency, currents, apparent and active power, output power factor, and load percentages.
    • Bypass status: Phase voltage, phase-to-phase voltage, frequency, and operating status.
    • Battery status: Estimated battery runtime, battery capacity, current, voltage and operating status.
    • Temperature information: On internal components.
    • Parameter information: Voltage range and frequency range information for input, bypass, and ECO.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?