Configure the Battery Settings
| NOTICE |
|---|
|
risk of equipment damage
Only trained personnel following the required training
must make modifications to the UPS system parameters.
Failure to follow these instructions can result in equipment damage.
|
- From the home screen of the display select .
- Set the Number of battery blocks in one battery string.
- Set the Total battery capacity.
- Set the Maximum charge current. Choose a value between 0.1C and 0.2C.
- Tap Save settings.
- Tap the arrow down symbol.
- Starting temp. compensation at (°C): Choose a value between 20 °C and 25 °C.
- Float charge temp. compensation (mV/°C/cell): Choose a value between 0 and 7.
- Select if Battery overtemperature protection should be enabled or disabled. If enabled, configure the following
settings:
- Battery overtemperature (°C): Choose a value between 40 °C and 45 °C.
- Battery overvoltage protection (V): Choose a value between 13 V and 15 V.
- Battery voltage warning (V): Choose a value between 13 V and 15 V.
- Tap Save settings.