990-91407D-001

Configure the Parameter Settings

NOTICE
risk of equipment damage
Only trained personnel following the required training must make modifications to the UPS system parameters.
Failure to follow these instructions can result in equipment damage.
  1. From the home screen of the display select Setting > UPS settings > Parameter settings.
  2. Select the Input source. Choose between Mains and Genset.
  3. Set the Output rated voltage. Choose between 220V, 230V, and 240V.
  4. Set the Output rated frequency. Choose between 50Hz and 60Hz.
  5. Select if the Power on wizard should be enabled or disabled.
  6. Tap Save settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?