990-91407D-001

Configure the Parallel Settings

NOTICE
risk of equipment damage
Only trained personnel following the required training must make modifications to the UPS system parameters.
Failure to follow these instructions can result in equipment damage.
  1. From the home screen of the display select Setting > Advanced settings > Parallel settings.
  2. Set the Number of parallel UPSs. Select a number between 2 and 4.
  3. Set the Number of par. redundant UPSs. Select a value between 0 and 3.
  4. Tap Save settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?