990-91407D-001

Configure the Network Settings

  1. From the home screen of the display select Setting > General settings > Network settings
  2. Set the Modbus ID. Select a value between 1 and 247.
  3. Set the Modbus baud rate for communication using the left and right arrows. Choose between 2400, 4800, 9600, and 19200.
  4. Select if connection via RS485 port should be enabled or disabled.
  5. Tap Save settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?