Operation Modes
Normal Mode
The UPS provides power to the connected load from mains. The UPS converts mains to conditioned power for the connected load while recharging the batteries (float or boost charge).
Battery Mode
The UPS transfers to battery mode if the mains supply fails. The UPS provides power to the connected load from the connected batteries for a finite period. When the mains supply returns, the UPS transfers back to normal mode.
Static Bypass Mode
The UPS supplies the load with power from the bypass source. If the conditions for normal or battery mode are not met, the load will be transferred from the inverter to the bypass source with no interruption in power to the load.
Maintenance Bypass Mode
In maintenance bypass mode, the mains is sent via the maintenance bypass disconnect device (MBB) to the load. Battery backup is not available in maintenance bypass mode.
ECO Mode
In ECO mode the UPS is configured to use static bypass mode as the preferred operation mode under predefined circumstances. The inverter is in standby in ECO mode and in case of interruption to the mains, the UPS transfers to battery mode and the load is supplied from the inverter.
Frequency Converter Mode
In frequency converter mode, the UPS presents a stable output frequency (at 50 or 60 Hz) and the static bypass switch is not available.
| NOTICE |
|---|
|
Risk of equipment damage or load drop
In frequency converter mode the UPS cannot run in static
bypass or maintenance bypass mode. Before turning the UPS into frequency
converter mode, you must contact a Schneider Electric-certified partner
to make sure that:
Failure to follow these instructions can result in equipment damage.
|
| NOTICE |
|---|
|
risk of load drop
When the unit output disconnect device UOB is opened while
the UPS is in frequency converter mode, the load will not be transferred,
but will be dropped.
Failure to follow these instructions can result in equipment damage.
|
Auto Restart
DANGER |
|---|
|
Hazard of electric shock, explosion, or arc flash
Always perform correct Lockout/Tagout before working on
the UPS. A UPS with auto restart enabled will automatically restart
when the mains supply returns.
Failure to follow these instructions will result in death or serious injury.
|
The batteries will reach end of discharge if the interruption to the mains is longer than the battery runtime available. When auto restart is enabled, the system will automatically restart when the mains returns.









DANGER