Configure the Battery Test Settings
| NOTICE |
|---|
|
risk of equipment damage
Only trained personnel following the required training
must make modifications to the UPS system parameters.
Failure to follow these instructions can result in equipment damage.
|
- From the home screen of the display select .
- Select if Battery test should be
performed automatically. If this function is enabled, configure the
following settings:
- Test schedule: Select the battery test interval: 1 month, 2 months, 3 months, 6 months, or 12 months.
- Date: Set the day of the month for the battery test to take place. Choose a value between 1 and 31.
- Time: Set the time of the day for the battery test to take place.
- Tap Save settings.
- Tap the arrow down.
- Set the Battery test - time: Select Enable to manually specify a battery test time limit.
- Set the Battery test - voltage: Select Enable to manually specify a battery test voltage limit.
- Tap Save settings.