990-91407D-001

Buzzer

NOTE: The buzzer is muted as default.

The buzzer is inside of the UPS. The buzzer will sound in the following instances:

  • UPS is on battery power: The buzzer will beep in intervals of 3.5 seconds and the beep will last 0.5 seconds.

  • UPS is on bypass: The buzzer will beep in intervals of 119 seconds and the beep will last 1 second.

  • Critical event: The buzzer will beep in intervals of 0.5 seconds and the beep will last 0.5 seconds. The buzzer will beep continuously until the critical event has been acknowledged and resolved.

  • Overload: The buzzer will beep in intervals of 0.26 seconds and the beep will last 0.24 seconds.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?