990-91407D-001

Configure the Output Dry Contacts

  1. From the home screen on the display select Setting > Advanced settings > Output dry contact and select the output dry contact that you want to configure. Configure the following for the input dry contact:
    1. Status: Set if the output dry contact is Open or Closed.
    2. Time-delay: Set the time delay (in seconds) for the output dry contact to activate.
    3. Function: Select the function of the input dry contact. Select between Disable, Common alarm,In normal operation, On battery, Static bypass, Output overload, Fan inoperable, Battery inoperable, Battery disconnected, Battery voltage low, Input out of tol., Bypass out of tol., EPO active, Maintenance bypass, Charging, Backfeed of M1, and Backfeed of M2.
    4. Click Save settings to save.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?