990-91407D-001

Perform a Battery Test

The battery test is used to test the health of the batteries.

  1. From the home screen on the display select Control > Battery test.
  2. Choose between the following tests:
    • 10 seconds: For a 10 seconds long discharge of the batteries.
    • 10 minutes: For a 10 minutes long discharge of the batteries.
    • End of discharge: For discharging the batteries until the end of discharge voltage is reached.
  3. Tap Confirm to start the battery test.
  4. Tap Abort to stop the battery test and tap Confirm to abort the test.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?