990-91407D-001

Export Data to a USB Drive

  1. From the home screen of the display select Service > Export data to USB.
  2. Open the front door of the UPS and insert a USB device in the USB port on the display.
  3. Select either to Export event logs or Export settings log.

    The Number of stored log entries and the Number of exportable log entries to USB are shown on the screen.

  4. Tap Export to export the log to the USB drive.
  5. Remove USB device from USB port.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?