990-91407D-001

Configure the Input Dry Contacts

  1. From the home screen on the display select Setting > Advanced settings > Input dry contact and select the input dry contact that you want to configure. Configure the following for the input dry contact:
    1. Status: Set if the input dry contact is Open or Closed.
    2. Time-delay: Set the time delay (in seconds) for the input dry contact to activate.
    3. Function: Select the function of the input dry contact. Select between Disable, INV ON, INV OFF, Battery inoperable, Genset ON, Custom alarm 1, Custom alarm 2,Disable ECO, and Forced INV OFF.
    4. Click Save settings to save.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?