Important Safety Instructions — SAVE THESE INSTRUCTIONS
Read these instructions carefully and look at the equipment to become familiar with it before trying to install, operate, service or maintain it. The following safety messages may appear throughout this manual or on the equipment to warn of potential hazards or to call attention to information that clarifies or simplifies a procedure.
DANGER |
|---|
|
DANGER indicates a hazardous situation which, if
not avoided, will result in death or serious injury.
Le non-respect de ces instructions provoquera la mort ou des blessures graves.
|
AVERTISSEMENT |
|---|
|
WARNING indicates a hazardous situation which,
if not avoided, could result in death or serious injury.
Le non-respect de ces instructions peut provoquer la mort, des blessures graves ou
des dommages matériels.
|
ATTENTION |
|---|
|
CAUTION indicates a hazardous situation which,
if not avoided, could result in minor or moderate injury.
Le non-respect de ces instructions peut provoquer des blessures ou des dommages matériels.
|
| AVIS |
|---|
|
NOTICE is used to address practices not related
to physical injury. The safety alert symbol shall not be used with
this type of safety message.
Le non-respect de ces instructions peut provoquer des dommages matériels.
|
Please Note
Electrical equipment should only be installed, operated, serviced, and maintained by qualified personnel. No responsibility is assumed by Schneider Electric for any consequences arising out of the use of this material.
A qualified person is one who has skills and knowledge related to the construction, installation, and operation of electrical equipment and has received safety training to recognize and avoid the hazards involved.
Per IEC 62040-1: "Uninterruptible power systems (UPS) -- Part 1: Safety Requirements," this equipment, including battery access, must be inspected, installed and maintained by a skilled person.
The skilled person is a person with relevant education and experience to enable him or her to perceive risks and to avoid hazards which the equipment can create (reference IEC 62040, section 3.102).
DANGER
AVERTISSEMENT
ATTENTION