EIO0000005603.01

Product Revision and QR Code

You can identify the product version (PV) and the software version (SV) from the product label.

You can also check the contents of this manual by using the QR code on the product label. Confirm the location of the QR code below and refer to the manual.

  1. This mark indicates that you can refer to wiring requirements in this manual by using the QR code. Refer to Wiring the Power Supply.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.