EIO0000005603.01

Installing M.2 SSD (SSD2)

In the M.2 SSD slot (SSD2), you can insert an M.2 SSD card as a secondary storage.

NOTE:
  • The SSD2 slot supports M.2 SSD Type 2280, 2252 and 2242. The key ID is Key B.

  • Although the SIM card slot on the SSD2 slot is visible, it is not available.

  1. Remove the maintenance hatch cover referring to Opening the Maintenance Hatch.
  2. Remove the screw in SSD2.
    NOTE: Using a Phillips screwdriver #1 is recommended.
  3. Insert an M.2 SSD card into the connector diagonally, then push from above.
  4. The following shows the screw position for each type of the M.2 SSD card.

    A. For Type 2280

    B. For Type 2252

    C. For Type 2242

  5. When inserting Type 2280 M.2 SSD card, tighten the screw removed in step 2 in the position indicated by A.

    When inserting Type 2242 or 2252, remove the spacer attached in the position indicated by A with a 5 mm box wrench.

    D. Spacer

    When inserting Type 2252, attach the spacer with a 5 mm box wrench in the position indicated by B, and tighten the screw removed in step 2 on it.

    When inserting Type 2242, attach the spacer with a 5 mm box wrench in the position indicated by C, and tighten the screw removed in step 2 on it.

    NOTE:
    • The necessary torque for the spacer is 0.35 N•m (3.1 lb-in).

    • The necessary torque for the screw is 0.2 N•m (1.8 lb-in).

  6. Place the maintenance hatch cover and tighten the screw.
    NOTE: The necessary torque is 0.2 N•m (1.8 lb-in).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.