EIO0000005603.01

Security Seal

This product has a security seal attached, which helps detect unauthorized repairs or modifications to the product. Once the security seal is removed or torn, it cannot be reapplied, increasing the product's security risk.

WARNING
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY
  • Do not remove or tear the security seal on the product.
  • Do not use products with removed or torn security seals.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTE: When the maintenance hatch cover is open for installing or replacing the M.2 SSD, M.2 card, or battery, it is recommended to take precautions to prevent unauthorized repairs or tampering through the maintenance hatch. This will help ensure that malicious individuals cannot gain access to the interior after the work is completed. Please note that the maintenance hatch cover should not be opened unnecessarily.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.