EIO0000005603.01

Part Numbers

Part Number List

Series

Display size

Part number

Harmony PSA6

12-inch wide

HMIPSA6AED18W11

15-inch

HMIPSA6A7D18W11

15-inch wide

HMIPSA6AFD18W11
HMIPSA65FD18W11
HMIPSA65FD2AW11

19-inch wide

HMIPSA65GD18W11
HMIPSA65GD2AW11

NOTE: All part numbers may be followed by any letter or number.

Part Number Configuration

The following describes the configuration of model numbers.

Digit Category Number Description
1-7 (Prefix) HMIPSA6  
8 CPU A Atom
5 Core i5
9 Size 7 15-inch
E 12-inch wide
F 15-inch wide
G 19-inch wide
10 Power D 24 Vdc
11 Main storage 1 M.2 SATA SSD 128 GB
2 M.2 NVMe SSD 256 GB
12 Memory 8 DIMM 8 GB
A DIMM 16 GB
13-15 Operating System W11 Windows 11 IoT Enterprise 2024 LTSC (64 bit)
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.