EIO0000005603.01

Opening the Maintenance Hatch

  1. Disconnect the power supply from this product.
  2. Touch the housing or ground connection (not the power supply) to discharge any electrostatic charge from your body.
  3. Place the product face down on a clean, flat, level surface.
  4. Remove 2 screws of the maintenance hatch.
    NOTE: Using a Phillips screwdriver #1 is recommended.
  5. Remove the cover.
  6. After installing the M.2 SSD or M.2 card, place the cover and tighten the screw.
    NOTE: The necessary torque is 0.2 N•m (1.8 lb-in).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.