EIO0000005603.01

Installing M.2-E Card

In the M.2-E slot (M.2-E), you can insert an M.2 Key E card for a WiFi/Bluetooth connection.

NOTE: The M.2-E slot supports M.2 Key E Type 2230.
  1. Remove the maintenance hatch cover referring to Opening the Maintenance Hatch.
  2. Remove the screw in M.2-E.
    NOTE: Using a Phillips screwdriver #1 is recommended.
  3. Insert an M.2 Key E card into the connector diagonally, then push from above.
  4. Tighten the screw removed in step 2.
    NOTE: The necessary torque is 0.2 N•m (1.8 lb-in).
  5. Place the maintenance hatch cover and tighten the screw.
    NOTE: The necessary torque is 0.2 N•m (1.8 lb-in).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.