EIO0000005603.01

LED Indication

Status LED

Color

State

Description

Green

ON

S0 (in operation)

Flashing

Screen is turned off.

Orange

ON

S3

Flashing

System is starting up.

Red

ON

S4, S4 (hybrid shutdown)*1, S5

-

OFF

G3 (power is off)

*1 S4 (hybrid shutdown) is S5 when Windows® fast startup is enabled.

Wake-up Events

The following is a table showing the statuses that are set to the normal startup (S0) state when each action is executed.

ACPI state

Power state

Power up

Power button is ON

Wake on LAN

Touch input

USB equipment*1

S3

Sleep

S4

Hibernate

S4 (hybrid shutdown)

Hibernate

S5

Soft off

G3

Mechanical off

*1 Limited to USB devices that support the remote wake-up function.

NOTE: If you turn on the power when G3 is set, it directly enters state S0.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.