EIO0000005603.01

Termination Resistor Setting

Termination resistor setting is necessary when using RS-422/485. The following describes how to set the termination resistor.
  1. Display the BIOS screen. Refer to Harmony PSA6 Windows System Setting User Guide.
  2. Select Advanced > NCT5525D Super IO Configuration > Serial Port 2 Configuration.
  3. In Termination resistors, select Enabled.
  4. Press the [F4] key.
  5. Select Yes in the Save & Exit Setup dialog box.
  6. The product is restarted.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.