EIO0000005603.01

Attaching USB Cable Clamp

When using a USB device, attach a USB cable clamp to the USB interface to prevent the USB cable from being disconnected.

NOTE: The USB cable clamp is an optional item (HMIZCCLUSA) and needs to be purchased separately.
WARNING
EXPLOSION HAZARD
  • Do not disconnect equipment while the circuit is live or unless the area is known to be free of ignitable concentrations.
  • Remove power before attaching or detaching any connectors to or from this product.
  • Ensure that power, communication, and accessory connections do not place excessive stress on the ports. Consider the vibration in the environment when making this determination.
  • Securely attach power, communication, and external accessory cables to the panel or cabinet.
  • Use only commercially available USB cables.
  • Use only non-incendive USB configurations.
  • Confirm that the USB cable has been attached with the USB cable clamp before using the USB interface.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTE: Watch your fingers. The edge of the clip is sharp.
  1. Mount the clip to the USB mark on the USB connector shell so that it overlaps. The clip matches a length of 27 to 43.5 mm (1.06 to 1.71 in) for the USB cable connector.
    NOTE: When installing clamps to reduce cable stress onto both the upper port and lower port, at the upper port overlay the clip on the side with the USB mark, and on the lower port the side without the USB mark. Make sure the ties do not interfere with the other.
  2. Align the clip and the USB cable connector shell. Adjust the position of the holes where the clip is attached. To ensure stability, select the clip-hole position that is closest to the base of the connector shell.

    A. Pass the tie through here.

  3. As shown, pass the tie through the clip hole. Next, turn the tie and pass it through the head so that the USB cable can pass through the center of the tie loop. The clip is now attached to the USB cable.
    NOTE:
    • Check the direction of the head beforehand. Make sure the USB cable is through the center of the tie loop and that the tie can pass through the head.

    • You can substitute the tie provided with HMIZCCLUSA or other commercially available ties with a width of 4.8 mm (0.19 in) and thickness of 1.3 mm (0.05 in).

  4. While pressing the grip on the clip, insert the cable from step 3 all the way into the USB host interface. Make sure that the tab of the clip is secured to the USB cable attached to this product.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.