EIO0000005603.01

RS-422

D-Sub 9 pin plug connector

Product side:

Pin No.

RS-422

Signal name

Direction

Description

1

TxD-

Output

Send data -

2

TxD+

Output

Send data +

3

RxD+

Input

Receive data +

4

RxD-

Input

Receive data -

5

SG

-

Signal ground (not isolated)

6

NC

-

No connection

7

NC

-

No connection

8

NC

-

No connection

9

NC

-

No connection

Shell

FG

-

Frame ground (common with SG)

Recommended jack screw is #4-40 (UNC).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.