EIO0000005603.01

Removing USB Cable Clamp

  1. When USB cables with the clamps are connected to both the upper port and lower port, remove the cable with the clamp from the upper port.
  2. Loosen the cable tie of the USB clamp in the lower port.
  3. Remove the cable.
  4. Remove the USB clamp.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.