EIO0000005603.01

RS-232C (COM1)

D-Sub 9 pin plug connector

Product side:

Pin No.

RS-232C

Signal name

Direction

Description

1

CD

Input

Carrier detect

2

RD (RXD)

Input

Receive data

3

SD (TXD)

Output

Send data

4

ER (DTR)

Output

Data terminal ready

5

SG

-

Signal ground (not isolated)

6

DR (DSR)

Input

Data set ready

7

RS (RTS)

Output

Request to send

8

CS (CTS)

Input

Send possible

9

CI (RI)

Input

Called status display

Shell

FG

-

Frame ground (common with SG)

Recommended jack screw is #4-40 (UNC).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.