EIO0000005603.01

Package Contents

Verify all items listed here are present in your package.

If you find anything damaged or missing, please contact customer support immediately.

WARNING
UNINTENDED EQUIPMENT OPERATION
Do not use damaged products or accessories.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
  1. HMIPSA6 model x 1

  2. Installation fasteners*1 (to install on a panel):

    4 pieces (for 12-inch wide model)

    8 pieces (for 15-inch, 15-inch wide and 19-inch wide)

  3. DC power connector x 1

  4. Connector to extend the power button x 1, refer to Parts Identification.

*1 There is no installation fastener prepared as a maintenance accessory. Please do not lose the fasteners included in your package.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.